2026-05-11 3:09 AM
Hello,
long time lurker, now with an issue that I would like to solve.
I developed a firmware that runs standalone without issue. I would like to use the secure manager on my STM32H573VI microcontroller.
I followed the procedures at this link: https://wiki.st.com/stm32mcu/wiki/Security:How_to_make_your_application_compatible_with_Secure_Manager
and I am able to run the python provisioning.py --sfi-flash command. Then from the cube ide I can debug my program that is written with cmake and the cubemx template.
Since I am using threadx I set TIM6 as a time base for the HAL.
What I observe is the following...
- if I run the application straight away, I do not see the tick increment.
- I set an __enable_interrupt() before HAL_Init() and I see that the tim6 interrupt is fired.
Then in the ISR, I see that with the first line of HAL_TIM_IRQHandler, when reading htim->Instance->DIER then I land in a BusFault_Handler.
I run out of ideas. No clue about how to deal with hit.
There is someone that solved a situation similar to this one?
thank you in advance
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.