2018-09-12 7:44 PM
I'm using a reed switch (a pulse per revolution) to measure the speed of a wheel. The sensor output is connected to PA12 which is TIM1_ETR pin. I connected it there by mistake in my final PCB. I would have to tweak the PCB if I want to change timer channel.
Is there a way that I can measure speed on this pin?
2018-09-12 8:12 PM
Configure TIM1 in External Count mode, using TIM1_ETR.
Set counter in maximal mode (TIM1->ARR = 0xFFFF), and then read the counter TIM1->CNT once a second, and subtract out the count from the prior read. Do the math using uint16_t variables.
2018-09-12 8:56 PM
Sorry for this question .. but I forgot to mention that channel 1 from Timer1 (PA8) is used as PWM generation. Does this affect what you explain above? I'm just starting to get involved with STM32 and CubeMx
2018-09-12 9:26 PM
So if you can't use it as a TIM input, consider using PA12 as an EXTI, generating an interrupt for each pulse.
2018-09-12 10:13 PM
So I think that I can set PA12 as an EXTI and update a variable each time the pulse is given. But I would need the time elapsed between pulses. Is there a way to find it out?
2018-09-13 4:49 AM
To what accuracy?
You could have TIM2 counting elapsed microseconds.
Or frankly just have the EXTI increment a counter you check every second or millisecond.
Sorry you don't mention a range of speeds/frequencies involved. 
2018-09-13 9:53 AM
It's low RPM application. The reed switch is located in a treadmill. I don't have the exact range of speed, but motors I'm using are around 3000 RPM max. Of course, this limit is not reached in treadmill applications