cancel
Showing results for 
Search instead for 
Did you mean: 

Rc522 library for STM32F030C8

droid nk
Associate II
Posted on January 05, 2018 at 14:03

Hello.

I've started using stm32f0 recently. I've been reading about the RFID technology and came across the famous MIFare cards and RC522 reader. I found many libraries and support for RC522 and arduino. I also found a library for stm32f103.

Are there any example code for reading and writing data onto the MI fare Classic card via Rc522 connnected to STM32F030 via SPI as i don't want to use Arduino. 

Also is there any library for rc522 compatible for stm32f030 which can assist me in sending data to the RC522 module?

I'm a new comer into the STM family so do not know much about it. Any little suggestion will also be of great assistance to me. 

Thank you.

#rc522 #mifare #stm32f030-spi #stm32f030
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0