cancel
Showing results for 
Search instead for 
Did you mean: 

Question about st Thread_Coap_MultiBoard example

Bkim.6
Associate II

Hi

i'm testing Thread_Coap_MultiBoard example and it works well as readme.txt explained.

but it's on m4(=cpu1) layer.

i have question for m0 behavior about mesh network.

i get a m0(=cpu0)'s serial log below

```

[0002283462] [MLE] [INFO]-MLE-----: Receive Advertisement (fe80:0:0:0:c8f5:87b:4ce2:d924,0x2c00)

[0002283464] [MLE] [INFO]-MLE-----: Route table updated

[0002283464] [MLE] [INFO]-MLE-----:   2c00 -> 6000, cost:1 1, lqin:3, lqout:3

[0002283465] [MLE] [INFO]-MLE-----:   5400 -> fc00, cost:0 16, lqin:0, lqout:0

[0002283466] [MLE] [INFO]-MLE-----:   6000 -> 2c00, cost:1 1, lqin:3, lqout:3

[0002283467] [MLE] [INFO]-MLE-----:   9000 -> 6000, cost:1 1, lqin:3, lqout:3

[0002283468] [MLE] [INFO]-MLE-----:   bc00 -> 6000, cost:1 1, lqin:3, lqout:3

```

Not like the above, can i change network topology as i want ?

if then, How can I do that?​

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0