cancel
Showing results for 
Search instead for 
Did you mean: 

Programming External RAM

lonnie
Associate II
Posted on November 19, 2008 at 07:26

Programming External RAM

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
lonnie
Associate II
Posted on May 17, 2011 at 12:52

What are all the available options to program external RAM? IAR provides a flashloader to program external flash via the debugger. Is there anything similar for programming external RAM?

I'm aware of the DFU tool, but are there any other options?

thanks

jilisegiar
Associate II
Posted on May 17, 2011 at 12:52

Refer to the following example:

FWLib\examples\FSMC\SRAM_DataMemory

jilisegiar
Associate II
Posted on May 17, 2011 at 12:52

What you mean by ''to program external ram with a binary file''. if I understand well you need to load your code into external RAM. Is it OK?

In this case you need to configure the FSMC before programming the external SRAM.

For more details, refer to:

http://www.st.com/mcu/modules.php?name=mcu&file=familiesdocs&FAM=110#Application Note

lonnie
Associate II
Posted on May 17, 2011 at 12:52

Thanks for the response jilisegiar.

I did see the sram data memory example, which is demonstrates how to use external ram for program data memory and internal SRAM for Stack.

I'm interested in having the ability to program external ram with a binary file. Similar in the way of how a flashloader is loaded in internal ram and fetches a binary file from the c-spy debugger, which it then programs external memory with.