cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with I2C and TIM1

karolina
Associate II
Posted on May 18, 2015 at 11:53

Hello!

I have downloaded Cube for stm32f091 and have some problems with I2C_TwoBoards_Com example.

The problem is frequency of I2C clock. In example is said that System Clock is 48MHz. And with macro 

&sharpdefine I2C_TIMING      0x00A51314

I2C clock is set to reach 1MHz speed. Bus as you can see in picture, it's not the case. Frequency is 500kHz. 

Could you tell me how to calculate constant to reach frequency 1MHz? 

Few days ago I tried to work with timer example, and there was also a problem with main clock. I guess the frequency is not set to 48MHz but some other. Did anyone had similar problem? How did you solve it?

http://www.deviantpics.com/image/LSy

Also the look of the signal is not rect, I guess the frequency is too high :/. Are my assumptions ok?

Thank you!

#stm32f091 #stm32f0-cube
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0