cancel
Showing results for 
Search instead for 
Did you mean: 

problem using (hal_stm32f4xx library) to restore value written to user configured flash after power reset

mahmuudesam
Associate II
Posted on March 19, 2015 at 12:07

can any one help me with this problem? I try to  save value in the user configured section of flash memory and restore it after power reset through hal_stm32f4xx library. I started debugging by reading the value from the programmed address without power reset and it was right. But then I tried to check the value after power reset so I ran this code . If the value is read correct (the led connected to GPIO_10) should turn on, but this didn't happen .

__attribute__((__section__(''.user_data''))) const uint32_t userConfig[64];

uint32_t testreadvalue=0;

uint32_t testwritevalue=6;

void testreadFlash(void)

{

    testreadvalue =*(uint8_t *)userConfig;

}

void testwriteFlash(void)

{

    HAL_StatusTypeDef status;

    status =    HAL_FLASH_Unlock();   // returns 

HAL

_OK

    FLASH->CR |= 0x1000000;

    FLASH_Erase_Sector(FLASH_SECTOR_2, VOLTAGE_RANGE_1);

    __HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP | FLASH_FLAG_OPERR | FLASH_FLAG_WRPERR | FLASH_FLAG_PGAERR | FLASH_FLAG_PGSERR );

    status = HAL_FLASH_Program(TYPEPROGRAM_HALFWORD, (uint32_t) userConfig, (uint64_t)testwritevalue);

   

// returns 

HAL

_OK

    while((*(uint8_t* )(userConfig))==0);

    status = HAL_FLASH_Lock();       

// returns 

HAL

_OK

}

int main(void)

{

    HAL_Init();

    MX_GPIO_Init();

    testreadFlash();

    if(testreadvalue==6)

      { HAL_GPIO_WritePin(GPIOB,GPIO_PIN_10,0);}            //power cycle the device  //TESTING

    else

      { testwriteFlash();}

       SystemClock_Config();

  

     while (1)

        {}

 }

and this is the part of the linker for the user configured flash

MEMORY   

{

// RAM 

default

  FLASH1 (rx) : ORIGIN = 0x08000000, LENGTH = 32k

  DATA (xrw) : ORIGIN = 0x08008000, LENGTH = 32k        

  FLASH (rx) : ORIGIN = 0x08010000, LENGTH = 512K-64k 

//others default

}

SECTIONS

{

    .user_data :

    {

      . = ALIGN(4);

         *(.user_data)

      . = ALIGN(4);

    } > DATA

}

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0