2020-06-11 4:23 AM
Im trying to write to and read data from 10 eeproms in parallel. I first transmit the data in parallel to all the eeproms via spi, I then read data in parallel by first transmitting the address of data stored in the eeprom and then transmitting dummy data in non blocking mode in order to pass a clock signal to eeprom and allow it to output data stored.
From the signals on my oscilloscope everything works perfectly, the eeprom outputs data I send it. However when trying to read the gpio pins in order to record data only the first 4 bits in every byte gets read as observed from debug mode.
Attached is my code and relevant pics.
Thanks for your help.
Edit: Solution in last post
uint8_t data_tx[6]={2,0,0,1,21,1}; //0,1,5,1 is data i send to store
uint8_t address_read[4]={3,0};
uint8_t write_en=6;
uint16_t dat[100];
uint8_t dummy[3]={0,0,0};
while (1)
{
//set write enable latch in parallel
GPIOA->ODR = 0x0000; // pull the CS pins low
HAL_SPI_Transmit(&hspi3,&write_en, 1, 10); //set write enable latch
GPIOA->ODR = 0xffff; // pull the CS pins high
HAL_Delay(10);
//write in parallel
GPIOA->ODR = 0x0000; // pull the CS pin low
HAL_SPI_Transmit(&hspi3,data_tx, 6, 10); //transmit addresses and data
GPIOA->ODR = 0xffff; // pull the CS pins high
HAL_Delay(10);
//read in parallel using ports
GPIOA->ODR = 0x0000; // pull the CS pins low
HAL_SPI_Transmit (&hspi3, address_read, 2, 10); // send address
HAL_SPI_Transmit_IT(&hspi3, dummy, 20);
for(int i = 0; i < 100; i++)
{
if((GPIOB->IDR & 0x01ff) >= 0x01f0)
{
dat[i] = (GPIOB->IDR & 0x01ff) ; //problematic
}
}
GPIOA->ODR = 0xffff; // pull the CS pins high
HAL_Delay(10);
}
Solved! Go to Solution.
2020-06-11 6:32 AM
I changed my while loop to this, it doesn't seem to work. Can you please correct me
while (1)
{
MX_SPI3_Init();
//set write enable latch in parallel
GPIOA->ODR = 0x0000; // pull the CS pins low
HAL_SPI_Transmit(&hspi3,&write_en, 1, 10); //set write enable latch
GPIOA->ODR = 0xffff; // pull the CS pins high
HAL_Delay(10);
//write in parallel
GPIOA->ODR = 0x0000; // pull the CS pin low
HAL_SPI_Transmit(&hspi3,data_tx, 6, 10); //transmit addresses and data
GPIOA->ODR = 0xffff; // pull the CS pins high
HAL_Delay(10);
//read in parallel using ports
GPIOA->ODR = 0x0000; // pull the CS pins low
HAL_SPI_Transmit (&hspi3, address_read, 2, 10); // send address
GPIO_InitTypeDef GPIO_InitStruct = {0}; //change SCK to gpio
GPIO_InitStruct.Pin = GPIO_PIN_10;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_PULLDOWN;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
for(int i = 0; i < 25; i++)
{
HAL_GPIO_TogglePin(GPIOC, GPIO_PIN_10);
if((GPIOC->ODR & 0x0400) == 0x0400)
{
dat[i] = (GPIOB->IDR);
}
HAL_Delay(1);
}
GPIOA->ODR = 0xffff; // pull the CS pins high
HAL_Delay(10);
/* USER CODE BEGIN 3 */
}
2020-06-11 7:24 AM
> it doesn't seem to work
What are the symptoms?
Did you observe the pins (SCK and some of the MISO/PBx)?
JW
2020-06-11 10:14 AM
while (1)
{
/* USER CODE END WHILE */
HAL_GPIO_DeInit(GPIOC, GPIO_PIN_10);
MX_SPI3_Init();
//set write enable latch in parallel
GPIOA->ODR = 0x0000; // pull the CS pins low
HAL_SPI_Transmit(&hspi3,&write_en, 1, 1); //set write enable latch
GPIOA->ODR = 0xffff; // pull the CS pins high
HAL_Delay(10);
//write in parallel
GPIOA->ODR = 0x0000; // pull the CS pin low
HAL_SPI_Transmit(&hspi3,data_tx, 6, 6); //transmit addresses and data
GPIOA->ODR = 0xffff; // pull the CS pins high
HAL_Delay(10);
//read in parallel using ports
GPIOA->ODR = 0x0000; // pull the CS pins low
HAL_SPI_Transmit(&hspi3, address_read, 2, 2); // send address
HAL_SPI_DeInit(&hspi3); //deinitialise spi
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_10, GPIO_PIN_RESET); //make sck a gpio
GPIO_InitTypeDef GPIO_InitStruct = {0};
GPIO_InitStruct.Pin = GPIO_PIN_10;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
for(int i = 0; i < 25; i++)
{
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_10, GPIO_PIN_SET);
if((GPIOC->ODR & 0x0400) == 0x0400)
{
dat[i] = ((GPIOB->IDR) & 0x03ff);
}
HAL_GPIO_WritePin(GPIOC, GPIO_PIN_10, GPIO_PIN_RESET);
}
GPIOA->ODR = 0xffff; // pull the CS pins high
HAL_Delay(10);
/* USER CODE BEGIN 3 */
}So it works now, I get a correct output on the oscilloscope. However, I dont think im sampling data GPIO correctly:
I transmit 3 bytes: 1,21,1 but this is what I see in debug mode:
What do u think is the issue?
2020-06-11 11:10 AM
Nevermind, this works now! I dont know why it started working all of a sudden