cancel
Showing results for 
Search instead for 
Did you mean: 

P-L496G-CELL02, Could the Quectel BG96 replaced with Quectel EC25-E module ?

AShiv.437
Associate II

I'm curious to Know before purchasing this Board a few things,

  1. Our need is , the Board shall be reliable to adapt the Other Quectel Modules as well like for Indian Bands i.e EC25-E modems from Quectel.
  2. The issue is in India, LTE-M is not operational, so we have to use it on 2.5 GPRS mode.
  3. I'm assuming that software/firmware would not have much effect if the modedm is replaced with EC25-E, the issue is the compatible Hardware board for connection.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0