2020-07-09 2:47 PM
I am trying to flash options bytes on a STM32H7 via the code below. Both the code snippets return HAL_ERROR from the HAL_FLASH_OB_Launch(). What am I doing wrong?
I am referring to the following STM32Cube example code: https://github.com/STMicroelectronics/STM32CubeH7/blob/master/Projects/STM32H743I-EVAL/Applications/IAP/IAP_Main/Src/flash_if.c#L301
This is the one to setup RDP:
if ( HAL_FLASH_Unlock() != HAL_OK ) { goto flash_lock; }
if ( HAL_FLASH_OB_Unlock() != HAL_OK ) { goto ob_lock; }
FLASH_OBProgramInitTypeDef ob_struct = {0};
// RDP on Flash bank 2
ob_struct.Banks = FLASH_BANK_2;
ob_struct.OptionType = OPTIONBYTE_RDP;
ob_struct.RDPLevel = OB_RDP_LEVEL_1;
// Program options bytes
HAL_FLASHEx_OBProgram(&ob_struct);
if ( HAL_FLASH_OB_Launch() != HAL_OK) { goto ob_lock; }
// Lock memory
HAL_FLASH_OB_Lock();
HAL_FLASH_Lock();
return OK;
ob_lock:
HAL_FLASH_OB_Lock();
flash_lock:
HAL_FLASH_Lock();
return ERR_PROTECT;This is the one to setup a secure area:
if ( HAL_FLASH_Unlock() != HAL_OK ) { goto flash_lock; }
if ( HAL_FLASH_OB_Unlock() != HAL_OK ) { goto ob_lock; }
FLASH_OBProgramInitTypeDef ob_struct = {0};
// Secure Area on bank 1 without erase when RDP reset
ob_struct.Banks = FLASH_BANK_1;
ob_struct.OptionType = OPTIONBYTE_SECURE_AREA;
ob_struct.USERType = OB_USER_SECURITY;
ob_struct.USERConfig = OB_SECURITY_ENABLE;
ob_struct.SecureAreaConfig = OB_SECURE_RDP_NOT_ERASE;
// First 3 sectors
ob_struct.SecureAreaStartAddr = ADDR_FLASH_BANK_1_SECTOR_0_START;//0x000;
ob_struct.SecureAreaEndAddr = ADDR_FLASH_BANK_1_SECTOR_3_START;//0x5DB;
// Program options bytes
HAL_FLASHEx_OBProgram(&ob_struct);
if ( HAL_FLASH_OB_Launch() != HAL_OK) { goto ob_lock; }
// Lock memory
HAL_FLASH_OB_Lock();
HAL_FLASH_Lock();
return OK;
ob_lock:
HAL_FLASH_OB_Lock();
flash_lock:
HAL_FLASH_Lock();
return ERR_PROTECT;
2020-07-09 4:35 PM
Be aware that RDP is a global flag and not a per-bank setting.
Look at the return value of HAL_FLASHEx_OBProgram to make sure it's successful.
2020-07-09 7:17 PM
Thanks for the response.
1) To confirm I do not need to set ob_struct.Banks = FLASH_BANK_1?
2) I have confirmed in both code samples the HAL_FLASHEx_OBProgram returns HAL_OK...
3) Do you have any other ideas for debugging this?
Appreciate your support.