cancel
Showing results for 
Search instead for 
Did you mean: 

One pulse mode

phuocnguyenhuu96
Associate III

Hello everyone.

I'm studying in stm32f40g eval and using timer in one pulse mode.

First I'm use the example code TIM_OnePulse and modify it. I'm add the One pulse OUTPUT in function TIM_Config and One pulse EXTERNAL TRIGGER in function TIM_T2IConfig. I want to see the pulse output in Led4 (pin PC7), TIM3_CH2 and external trigger I use is rising edge in button wakeup, TIM5_CH1.

After modify, I download code into the kit but it doesn't work.

Please help me with this problem. Thank you.

Here is my code.

#include "main.h"

TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;

TIM_ICInitTypeDef    TIM_ICInitStructure;

TIM_OCInitTypeDef    TIM_OCInitStructure;

uint16_t uhPrescalerValue = 0;

static void TIM_Config(void);

static void TIM_T2IConfig(void);

int main(void)

{

 TIM_Config();

TIM_T2IConfig();

 uhPrescalerValue = (uint16_t)((SystemCoreClock / 2) / 42000000) - 1;

  

 /* Time base configuration */

 TIM_TimeBaseStructure.TIM_Period = 65535;

 TIM_TimeBaseStructure.TIM_Prescaler = uhPrescalerValue;

 TIM_TimeBaseStructure.TIM_ClockDivision = 0;

 TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

 TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure);

 /* TIM4 PWM2 Mode configuration: Channel1 */

 TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM2; // enable pwm mode 2 by writing OC1M = 111 in the TIMx_CCMR1 res

 TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; // compare enable

 TIM_OCInitStructure.TIM_Pulse = 16383; // compare value

 TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; // output compare state high

 TIM_OC1Init(TIM3, &TIM_OCInitStructure);

 /* TIM4 configuration in Input Capture Mode */

 TIM_ICStructInit(&TIM_ICInitStructure);

 TIM_ICInitStructure.TIM_Channel = TIM_Channel_2; 

 TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising; // TI2 rising edge is detected

 TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI;

 TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1; // capture detected each edge

 TIM_ICInitStructure.TIM_ICFilter = 0;

 TIM_ICInit(TIM5, &TIM_ICInitStructure);

 /* One Pulse Mode selection */

 TIM_SelectOnePulseMode(TIM3, TIM_OPMode_Repetitive);

 TIM_SelectInputTrigger(TIM5, TIM_TS_TI2FP2);

 TIM_SelectSlaveMode(TIM5, TIM_SlaveMode_External1);

// TIM_Cmd(TIM3,ENABLE);

 while (1)

 {

 }

}

static void TIM_Config(void) // ONE PULSE OUTPUT

{

 GPIO_InitTypeDef GPIO_InitStructure;

RCC->APB1ENR=RCC_APB1ENR_TIM3EN;

RCC->AHB1ENR=RCC_AHB1ENR_GPIOCEN;

  

 GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7; 

 GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; 

 GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; 

 GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; 

 GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; 

 GPIO_Init(GPIOC, &GPIO_InitStructure); 

 GPIO_PinAFConfig(GPIOC, GPIO_PinSource7, GPIO_AF_TIM3);  

}

static void TIM_T2IConfig(void) // EXTERNAL TRIGGER

{

GPIO_InitTypeDef GPIO_InitStructure;

RCC->AHB1ENR=RCC_AHB1ENR_GPIOAEN;

RCC->APB1ENR=RCC_APB1ENR_TIM5EN;

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; 

 GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; 

GPIO_Init(GPIOA, &GPIO_InitStructure);

 GPIO_PinAFConfig(GPIOA, GPIO_PinSource0, GPIO_AF_TIM5);

}

#ifdef USE_FULL_ASSERT

void assert_failed(uint8_t* file, uint32_t line)

{

 while (1)

 {}

}

#endif

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Khouloud GARSI
ST Employee

Hi @phuocnguyenhuu96​ ,

Could you please precise for which reason you're using two timers ?

The program is confusing: For example you're configuring channel 2 for timer 5 while in your description you mentioned that timer 5 channel 1 will be used. Please check your shared code.

Khouloud.