2018-04-10 11:47 PM
Hi all,
I am trying to put my nucleo F042 into standby mode.
I have a very simple configuration (no GPIOs).
The MCU enters Standby mode after doing all the inits.
I measure the current on JP1 but it gives me something like 700uA where the datasheet says ~3uA.
I need some help with this . I must be missing something..
Here is the code :
int main(void)
{ /* USER CODE BEGIN 1 *//* USER CODE END 1 */
/* MCU Configuration----------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init(); /* USER CODE BEGIN 2 *//* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */ while (1) { GPIO_InitTypeDef GPIO_InitStruct; GPIO_InitStruct.Pin = GPIO_PIN_All; GPIO_InitStruct.Mode = GPIO_MODE_ANALOG; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct); HAL_GPIO_Init(GPIOF, &GPIO_InitStruct); HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); HAL_SuspendTick(); HAL_PWREx_DisableVddio2Monitor(); HAL_PWR_DisableBkUpAccess(); HAL_PWR_DisablePVD(); HAL_PWR_DisableSEVOnPend(); HAL_PWR_DisableSleepOnExit(); HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN1); HAL_RCC_DeInit(); __HAL_RCC_CRC_CLK_DISABLE(); __HAL_RCC_DMA1_CLK_DISABLE(); __HAL_RCC_SRAM_CLK_DISABLE(); __HAL_RCC_GPIOF_CLK_DISABLE(); __HAL_RCC_GPIOB_CLK_DISABLE(); __HAL_RCC_GPIOA_CLK_DISABLE(); HAL_DeInit(); RCC_OscInitTypeDef s_RCC_OscInitStruct;/**Initializes the CPU, AHB and APB busses clocks
*/ s_RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_NONE; s_RCC_OscInitStruct.HSEState = RCC_HSE_OFF; s_RCC_OscInitStruct.LSIState = RCC_LSI_OFF; s_RCC_OscInitStruct.PLL.PLLState = RCC_PLL_OFF; s_RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE; s_RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL2; s_RCC_OscInitStruct.PLL.PREDIV = RCC_PREDIV_DIV1; if (HAL_RCC_OscConfig(&s_RCC_OscInitStruct) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); } HAL_PWR_EnterSTANDBYMode();/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */}
Thanks for your help.
A.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.