cancel
Showing results for 
Search instead for 
Did you mean: 

ns timing of sequence of external events

NWark.1
Associate II

Hello - I am looking for a solution that can time a sequence of external events (combination of rising and falling edges). The events can occur as close as every ~10ns. The max number of events in the sequence is of the order of 100. After this there can be a long delay. I am looking for <2ns resolution on the timestamps. Can you suggest a solution for this? Thanks!

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
berendi
Principal

HRTIM on the STM32H74x/H75x series comes close to your requirements.

There are capture counters with 480 MHz resolution, i.e. 2.083 ns. I have some doubts though, the external triggers might be sampled at 240 MHz only, and DMA might not be able to store the capture values quickly enough, but I might be wrong, so you can give it a try.

Another idea, if you can find a fast external serial to parallel converter that can convert the input to 16 parallel outputs, which can then be connected to a 16 bit GPIO port of the MCU, where a couple of hundred kilobytes worth of captured samples can be stored and examined at the end of the burst. I don't think that the MCU could provide all the clocks needed for that, so you'd probably need some external circuitry for that. I think it could work with the MCU sampling the parallel port at maybe every 15 MCU clock cycles.

View solution in original post

7 REPLIES 7

Going to be hard pressed to achieve with a General Purpose MCU.

TI has an interesting ToF measurement chip, but that's probably not going to be good for a stream of pulses.

Perhaps look at what people use for pattern buffers on logic-analyzers, something that can sample with high resolutions, and can be pulled out and measured at a more leisurely pace.

Other than that perhaps some custom hw, using an FPGA, CPLD, etc.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
NWark.1
Associate II

Thanks for the suggestions. I will follow up on them.

I was hoping that the STM32H7 with 480MHz clock speed might be able to get close to this. I noticed the high resolution timer resolution is 2.1ns.

NWark.1
Associate II

As a follow up, I noticed that the STM32F334 seems to have a resolution of 217ps on the high resolution timer. Is this a possible option for timing multiple events as long as I can read the timer capture register before the next event occurs (10+ns later)?

berendi
Principal

HRTIM on the STM32H74x/H75x series comes close to your requirements.

There are capture counters with 480 MHz resolution, i.e. 2.083 ns. I have some doubts though, the external triggers might be sampled at 240 MHz only, and DMA might not be able to store the capture values quickly enough, but I might be wrong, so you can give it a try.

Another idea, if you can find a fast external serial to parallel converter that can convert the input to 16 parallel outputs, which can then be connected to a 16 bit GPIO port of the MCU, where a couple of hundred kilobytes worth of captured samples can be stored and examined at the end of the burst. I don't think that the MCU could provide all the clocks needed for that, so you'd probably need some external circuitry for that. I think it could work with the MCU sampling the parallel port at maybe every 15 MCU clock cycles.

The capture resolution is still the same as the timer clock, 144 Mhz i.e. 6.94 ns.

From the reference manual

The high-resolution is not available for the following features

• Timer counter read and write accesses

• Capture unit

Thanks for clarifying.

NWark.1
Associate II

Thanks for the suggestions, that is very helpful.