cancel
Showing results for 
Search instead for 
Did you mean: 

North American STM32F7 seminar series

Posted on February 26, 2016 at 19:22

http://www.st.com/web/en/learning/seminar/stm32f7-seminar

Can I please strongly implore ST to do this with the 

http://www.st.com/web/en/catalog/mmc/FM141/SC1169/SS1858

 parts, and not the parts you announced in 

http://www.st.com/web/en/press/p3606s

.

For all the time-to-market posturing, ATMEL beat you to the market with a Cortex-M7 solution, and delivered the full ARM M7 implementation with the DP-FPU not SP-FPU, 300 MHz not 216 MHz, and 2MB not 1MB of FLASH.

The STM32F765, 7x7 and 7x9 are suppose to be fully released beginning May 2016, and these need to be the parts you show-case at the seminars, not DISCO boards with the older parts that you indicated were going to be used during the webinar yesterday. I think that would be a strategic mistake.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0