nandFlash via FSMC + interrupts
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-01-18 1:23 AM
Posted on January 18, 2018 at 10:23
Hello, I'am using STM32F746IG and I have a problem with writing data to the Nand Flash memory via the FSMC . When I generate a project with CubeMx, configuring only the flash memory, everything works, i.e. writing, reading, erasing, reading ID etc. The problem starts when I add TIMER to the project (or anything that generates an interrupt), then in the pages appears mistakes. Could this look like a connection to the __DSB barrier? What happens when __DSB is executing and the interrupt call?
#interrput #fsmc #nand-flash #__dsb
Labels:
- Labels:
-
FMC-FSMC
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0