cancel
Showing results for 
Search instead for 
Did you mean: 

More than one DSMPS on one MCU

DavidNaviaux
Senior II

I have developed a custom controller that uses the STM32G474RE to regulate the output voltage of two power supplies.

I am now developing the code to implement a peak-current mode controller for each of the two power supplies.  Is there a way that I can use the one FMAC to implement the required filtering for both power supplies?

If not, I suppose that I can use PID control on one of the two power supplies.

Any suggestions would be welcome...

Thank you,

David

 

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0