Skip to main content
kjepsen9
Associate III
July 27, 2009
Question

MircorFramwork

  • July 27, 2009
  • 6 replies
  • 1116 views
Posted on July 27, 2009 at 19:08

MircorFramwork

    This topic has been closed for replies.

    6 replies

    kjepsen9
    kjepsen9Author
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:18

    Hello,

    Just now we are talking about uC linix...

    Has anyone thought about port the MS Microframework?

    I defently think it is possibly to run on the 3210E Eval board.

    Howcome all the external RAM/Flash is taken of the new Eval board for connectivity line?

    Kasper

    kjepsen9
    kjepsen9Author
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:18

    These ppl can do it:

    http://www.ghielectronics.com/product/113

    Kasper

    st3
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:18

    Quote:

    I defently think it is possibly to run on the 3210E Eval board.

    On what basis do you think that?

    kjepsen9
    kjepsen9Author
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:18

    Hello,

    No, but compared to the specs in the link i gave the 3210E eval board has many more features + RAM/ROM...

    And the other i believe is the ARM7TDMI..

    Kasper

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:18

    Hi,

    You can visit

    http://www.microsoft.com/netmf/hardware/default.mspx

    http://www.microsoft.com/downloads/details.aspx?displaylang=en&FamilyID=42ce8508-ff00-4ab8-8495-df587d77a8f2

    The Micro Framework Porting Kit supports the adaptation of the platform to specific hardware for processors using the RealView, Keil and GCC toolchains for the ARM processors (including Cortex)...

    Cheers,

    STOne-32.

    st3
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:18

    Quote:

    These ppl can do it:

    http://www.ghielectronics.com/product/113

    Yes - but on different hardware.

    Have you specifically verified that the 3210E Eval board has the necessary resources to support the micro framework?

    In fact, what are the minimum resources necessary to support the micro framework?

    [ This message was edited by: st7 on 24-07-2009 18:37 ]