cancel
Showing results for 
Search instead for 
Did you mean: 

minimum HCLOK for USB OTG FS

Barbie
Associate II
Posted on September 01, 2013 at 09:24

I use today HCLK of 120Mhz taken from the systemclk of 120Mhz (prescale by 1), and active USB OTG FS no problem.

To save power I want to go as much as possible low with the freq, when not during fast operations, and go back to 120Mhz for fast operations.

I read in the manual that the HCLK should be more then 14.2Mhz for USB OTG FS to work.

So I try to go to 15Mhz by prescale the systemclk by 8 (from 120Mhz). I also read that I need to stratch USB response time to IN tokens so I do so and set it to 0x0F.

It is writen like this:

        /* HCLK = SYSCLK / 8*/

    RCC->CFGR &=  ~(RCC_CFGR_HPRE); // clear AHB prescaler

    RCC->CFGR |= RCC_CFGR_HPRE_DIV8; // get Down not lower then 15Mhz for UART BAUD RATE but also for USB FS OTG proper operation

  /* keep PCLK2 stay at same original freq */

    RCC->CFGR &=  ~(RCC_CFGR_PPRE2);

    RCC->CFGR |= RCC_CFGR_PPRE2_DIV1;

  /* keep PCLK1 stay at same original freq */

    RCC->CFGR &=  ~(RCC_CFGR_PPRE1);

    RCC->CFGR |= RCC_CFGR_PPRE1_DIV1;

  

    /* Setup SysTick Timer for 10ms interrupts according new HCLK */

    if (SysTick_Config((SystemCoreClock/8) / 100))

     {

      /* Capture error */

      while (1);

     }

    USB_OTG_dev.regs.GREGS->GUSBCFG &= ~(0xF << 10);

    USB_OTG_dev.regs.GREGS->GUSBCFG |= 0xF <<10;

I also check what is the new freq by operating

RCC_GetClocksFreq(&RCC_ClockFreq);

and see I get HCLK 15Mhz .

and I get the right setting in the USB stratch time.

But after doing so the USB not recognize on the PC.

I try to do the freq adjustment before and after USB init but not help.

When I pick HCLK of 30Mhz it is work O.K.

What could be the reason?

Bar.
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0