cancel
Showing results for 
Search instead for 
Did you mean: 

Microcontroller Clock Output pin MCO

waldin80
Associate II
Posted on July 27, 2010 at 11:08

Microcontroller Clock Output pin MCO

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
waldin80
Associate II
Posted on May 17, 2011 at 14:00

Ok, so to watch 72MHz sysclk signal I must to select in RCC_CFGR.MCO=111 to see PLL clock divided by 2 to see 36MHz, because the maximum speed of GPIO write.

Thks.

To answer another question my answer was that it is normal to see 72,70MHz instead 72MHz teorical.

Thks to all dudes

0690X0000060MlEQAU.gif