2010-09-28 5:09 AM
Mems on stm3210C eval
2011-05-17 5:09 AM
You can start with
http://www.st.com/stonline/products/literature/ds/12726/lis302dl.htm
if you have not done so.2011-05-17 5:09 AM
There is working mems driver code in the eval board firmware:
http://www.st.com/stonline/products/support/micro/files/stm3210c-eval_fw.zip
2011-05-17 5:09 AM
Thanks for the answer. I've read all theses docs; But it is not really helping. I'd rather have some C code to understand how I2C works with the IO Expander (which is where i'm stuck and what I wish to understand). The better would be a very basic example using ST libs.
Best Regards,
2011-05-17 5:09 AM
Hello,
thanks Tonyf, I've also seen this code but it just configure the interupt pin. It doesn't seem to demonstrate how to get datas thought I2C. Besides, when I run this demo, no action seems related to the MEMS.
Also, in the code, the configuration is done thought IOE_2_ADDR and, according to my readings, it is IOE_1_ADDR.
IOE_IOPinConfig(IOE_2_ADDR, (uint32_t)(MEMS_INT1_PIN | MEMS_INT2_PIN), Direction_IN);
/* ENABLE the alternate function for the Joystick pins */ IOE_IOAFConfig(IOE_2_ADDR, (uint32_t)(MEMS_INT1_PIN | MEMS_INT2_PIN), ENABLE); /* Configure the IOs to detect Falling and Rising Edges */ IOE_IOEdgeConfig(IOE_2_ADDR, (uint32_t)(MEMS_INT1_PIN | MEMS_INT2_PIN), (uint32_t)(EDGE_FALLING | EDGE_RISING));
2011-05-17 5:09 AM
2011-05-17 5:09 AM
The IOE_Config() function configures the peripherals, this should be calledbefore calling other IOE... functions. Have a look through the code for this function for interrupt and I2C initialisation.
For reference, the code below works on my STM3210C, this is based on the example code. /**
* @brief Main program.
* @param None
* @retval None
*/
int main(void)
{
uint8_t memsData;
char lcdLine[20];
uint32_t revid, devid;
uint16_t lpCnt; /* Setup the microcontroller system. Initialize the Embedded Flash Interface,
initialize the PLL and update the SystemFrequency variable. */
SystemInit();
/* SysTick end of count event each 10ms with input clock equal to 9 MHz (HCLK/8, default) */
SysTick_Config(SystemFrequency / 100);
/* Init Debug Trace functions */
#ifdef DEBUG_TRACE_ENABLED
initDefaultDebugTrace();
printf(''Sys Start OK
'');
#endif /* Initialize LEDs and push-buttons mounted on STM3210X-EVAL board */
STM_EVAL_LEDInit(LED1);
STM_EVAL_LEDInit(LED2);
STM_EVAL_LEDInit(LED3);
STM_EVAL_LEDInit(LED4);
STM_EVAL_PBInit(Button_WAKEUP, BUTTON_MODE);
STM_EVAL_PBInit(Button_TAMPER, BUTTON_MODE);
STM_EVAL_PBInit(Button_KEY, BUTTON_MODE);
/* Initialize the LCD */
STM3210C_LCD_Init();
/* Clear the LCD */
LCD_Clear(Blue);
/* Set the LCD Back Color */
LCD_SetBackColor(Blue);
/* Set the LCD Text Color */
LCD_SetTextColor(White);
/* Configure the IO Expander */
if (IOE_Config() == IOE_OK)
{
LCD_DisplayStringLine(Line0, ''IO Expander OK'');
}
else
{
LCD_DisplayStringLine(Line0, ''IO Expander FAIL'');
LCD_DisplayStringLine(Line1, ''Please Restart board'');
while(1);
} /* Configure MEMS */
memsData = I2C_ReadDeviceRegister(MEMS_I2C_ADDR, MEMS_Who_Am_I);
if (memsData == MEMS_DEVICE_ID)
{
LCD_DisplayStringLine(Line1, ''MEMS comms OK'');
}
else
{
LCD_DisplayStringLine(Line1, ''MEMS comms FAIL'');
LCD_DisplayStringLine(Line2, ''Please Restart board'');
while(1);
}
/* Power up MEMS */
if (I2C_WriteDeviceRegister(MEMS_I2C_ADDR, MEMS_Ctrl_Reg1, 0x47) == IOE_OK)
{
LCD_DisplayStringLine(Line2, ''MEMS powerup OK'');
}
else
{
LCD_DisplayStringLine(Line2, ''MEMS powerup FAIL'');
LCD_DisplayStringLine(Line3, ''Please Restart board'');
while(1);
} revid = DBGMCU_GetREVID();
devid = DBGMCU_GetDEVID();
sprintf(lcdLine, ''Rev %d Dev %d '', revid, devid);
LCD_DisplayStringLine(Line9, (uint8_t*)lcdLine); /* Set the LCD Text Color */
LCD_SetTextColor(Cyan); /* Draw graph borders */
LCD_DrawRect(120, 120, 18, 120);
LCD_DrawRect(144, 120, 18, 120);
LCD_DrawRect(168, 120, 18, 120);
LCD_DrawLine(139, 60, 5, Vertical);
LCD_DrawLine(163, 60, 5, Vertical); LCD_DisplayStringLine(Line4, ''64=1G +/-2G''); /* Set the LCD Text Color */
LCD_SetTextColor(Green); #ifdef DEBUG_TRACE_ENABLED
printf(''LCD & MEMS initialised OK
'');
#endif lpCnt = 0; /* Main Loop */
while(1)
{
/* Clear old bar graph lines */
LCD_SetTextColor(Blue);
LCD_DrawLine( 121, (uint16_t)(60 - memsX/2), 16, Vertical);
LCD_DrawLine( 145, (uint16_t)(60 - memsY/2), 16, Vertical);
LCD_DrawLine( 169, (uint16_t)(60 - memsZ/2), 16, Vertical);
LCD_SetTextColor(Green); /* Read X */
memsX = (int8_t)(I2C_ReadDeviceRegister(MEMS_I2C_ADDR, MEMS_OutX));
sprintf(lcdLine, ''MEMS X %+2d '', memsX);
LCD_DisplayStringLine(Line5, (uint8_t*)lcdLine);
LCD_DrawLine( 121, (uint16_t)(60 - memsX/2), 16, Vertical); /* Read Y */
memsY = (int8_t)I2C_ReadDeviceRegister(MEMS_I2C_ADDR, MEMS_OutY);
sprintf(lcdLine, ''MEMS Y %+2d '', memsY);
LCD_DisplayStringLine(Line6, (uint8_t*)lcdLine);
LCD_DrawLine( 145, (uint16_t)(60 - memsY/2), 16, Vertical);
/* Read Z */
memsZ = (int8_t)I2C_ReadDeviceRegister(MEMS_I2C_ADDR, MEMS_OutZ);
sprintf(lcdLine, ''MEMS Z %+2d '', memsZ);
LCD_DisplayStringLine(Line7, (uint8_t*)lcdLine);
LCD_DrawLine( 169, (uint16_t)(60 - memsZ/2), 16, Vertical); /* Read Status Register */
memsData = I2C_ReadDeviceRegister(MEMS_I2C_ADDR, MEMS_Status_Reg);
sprintf(lcdLine, ''Status %X'', memsData);
LCD_DisplayStringLine(Line8, (uint8_t*)lcdLine); #ifdef DEBUG_TRACE_ENABLED
if ( (++lpCnt % 20) == 0 )
{
printf(''Cycle %d completed OK
'', lpCnt );
}
#endif /* 100mSec delay */
Delay(10);
}
}
2011-05-17 5:09 AM
Thanks for answer ... this damn sharepoint forum alert didn't work :(
I found also a way to works with mems by adpating the eeprom demo but it doesn't use interrupt yet.
I'll try your code and finish to debug mine and post result here.