2015-01-14 6:09 AM
I have used the STM32_USB_HOST_Library V2.1.0 (19-March-2012) on STM32F105 for implement Mass Storage Host class.
The file system is has been implemented with FatFs Module Source Files R0.07e.
The my problem is that not all pen drive are recognized! The symptom is that the USB Host core main state machine process (USBH_Process) remains in the HOST_ENUMERATION state! Below the list of pen drive tested:Made Capacity File System Cluster size Vel. Read Vel. Write Compatible
Kingston 14,42 GB FAT32 8 KB 18,12 MB/s 1,44 MB/s YES Gudget 0,94 GB FAT 16 KB 15,20 MB/s 5,43 MB/s YES Kingston 0,93 GB FAT32 4 KB 12,13 MB/s 2,05 MB/s YES Laser 3,76 GB FAT32 4 KB 15,60 MB/s 2,48 MB/s NO Verbatim 7,50 GB FAT32 4 KB 13,60 MB/s 3,85 MB/s NO Verbatim 7,28 GB FAT32 4 KB 19,8 MB/s 10,20 MB/s NOany idea?
Thanks
2015-01-15 12:21 AM
Maybe not software? Maybe the larger faster parts use more power and your power supply is insufficiently decoupled, underpowered and drooping or noisy?
2015-01-15 5:54 AM
How can I verify this?
Thanks2015-01-16 12:31 AM
Is it custom hardware? You could look at supply with an oscilloscope - add additional decoupling to USB stick supply - involve the circuit designer - read the power supply chip data sheet.
2015-01-16 3:12 AM
I resolved!
Is not the hardware problem, but is interrupt priority problem. I have set the the usb interrupt priority at top.2015-01-16 4:54 AM
Did you previously have higher priority interrupts that blocked? If so, what length of time do you think is critical?
Pleased to hear you now have it working.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.