Skip to main content
Matthew Force
Visitor II
May 24, 2018
Question

Masking unwanted callbacks

  • May 24, 2018
  • 1 reply
  • 514 views
Posted on May 24, 2018 at 14:07

The following is CubeMX generated code (STM32L051) for TIM interrupts.  I am interested in the capture callback from a different TIM channel configured for IC but I am also getting OC_Delay and PWM_PulseFinished callbacks firing.  Without modifying the auto-generated code, how do I disable the TIM interrupts I do not want while still enabling the one I do?

void HAL_TIM_IRQHandler(TIM_HandleTypeDef *htim)

{

...

if(__HAL_TIM_GET_FLAG(htim, TIM_FLAG_CC2) != RESET)

{

if(__HAL_TIM_GET_IT_SOURCE(htim, TIM_IT_CC2) !=RESET)

{

__HAL_TIM_CLEAR_IT(htim, TIM_IT_CC2);

htim->Channel = HAL_TIM_ACTIVE_CHANNEL_2;

/* Input capture event */

if((htim->Instance->CCMR1 & TIM_CCMR1_CC2S) != 0x00U)

{

HAL_TIM_IC_CaptureCallback(htim);

}

/* Output compare event */

else

{

HAL_TIM_OC_DelayElapsedCallback(htim);

HAL_TIM_PWM_PulseFinishedCallback(htim);

}

htim->Channel = HAL_TIM_ACTIVE_CHANNEL_CLEARED;

}

}

...

}

    This topic has been closed for replies.

    1 reply

    Rock Deng
    Associate III
    November 1, 2018

    Actually, you need do nothing. Those callback functions called in HAL_TIM_IRQHandler are all __weak function, they will do nothing until you redefine/rewrite them.