2017-09-07 8:52 AM
Hello,
i would like to know what is the thermal resistance Rjc for a package LQFP-64. I didn't saw the value in the datasheet and i need it to know the Tj temperature, when PDmax is 0.1mW and my case is 90degrees.
Thanks you
2017-09-07 9:43 AM
ST spreads or hides chip temperature data in many documents, it is difficult to find exact figures. But I would quess that the temperature is very close to the external temp. 0.1mW is a very small power. For a 746 chip LQFP100 it was 43 degrees per watt.
2017-09-07 11:12 AM
For critical commercial designs I'd strongly recommend working with an FAE who can get the answers, test data and characterization needed.
2017-09-07 2:41 PM
ST spreads or hides chip temperature data in many documents, it is difficult to find exact figures
I didn't find it particularly difficult to find; it's simply in the DS for the given model. Not that surprisingly, it's (slightly) dependent on particularities of each chip, not just the package itself. Two randomly selected examples:
JW