2018-06-20 5:30 AM
Hi there,
I am developing a custom board (F103 and CMWX1ZZABZ LoRa module). I have that the lora module goes into stop mode alone but every time I have tried to measure power consumptionbut it is always 1.22 mA when module should be in stop mode.
I am using B-L072Z-LRWAN1 AT_slave program to flash the module. I have deactivated all traces, debug and leds but it keeps measuring too much.
What else should I try? Is there a binary out there to flash the AT version without messing with other projects?
2018-08-09 9:58 PM
Sorry, bumping old zombie unanswered questions off my feed