2018-01-18 12:45 AM
Good morning,
I got an issue with the ROP-Level (read out protection) and therefore the MC is locked for further flash – actions. The power supply has been interrupted during an flash – action. I assume that this is the reason why the ROP level has been set to 1.
However, I checked the common sources and pages for troubleshooting / handling for that issue. I tried the ST-Link utility tool and the J-Link command line / J-Link unlock tool.
I’m not able to reset the ROP level to 0, neither with the on or the other tool. Please see the attached screenshots (two for J-Link and 5 for ST-Link).May you can give me a few hints to fix that issue?
Kind Regards, Kusche2018-02-06 2:04 AM
Kindly reminder
2018-02-06 2:27 AM
Tried a mass erase within the ST-Link tool ?
Didn't check recently, but former versions had such a menu point.
Or the system bootloader via the Boot0/Boot1 pin trick ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.