cancel
Showing results for 
Search instead for 
Did you mean: 

LCD UC1608 SPI S8

rudex
Associate
Posted on November 02, 2012 at 13:17

I have a problem with the initialization of the display AGG240128A05-FHW-R

I do not know what could be wrong. Maybe someone has an idea?

code:

 &sharpinclude ''GLCD_240x128.h''

&sharpinclude ''STM32F10x.h''

 

 

/*

  GPIO_SetBits(DrivePort_B, BM1);     //DelayLCD(0xFF);

  GPIO_SetBits(DrivePort_B, BM0);     //DelayLCD(0xFF);

*/

//----------------------------------------------------------------------------------------------------------

void GLCD_Init(void){

 

    //Display initialisaton

  volatile unsigned long int i;

 

  GPIO_ResetBits(DrivePort_B, RES);    //RES=0

  GLCD_delay(100);

  GPIO_SetBits(DrivePort_B, RES);        //RES=1

    GLCD_delay(100);

  //CD=0 wysylanie komend

    GPIO_ResetBits(DrivePort_B, CS);

    GPIO_ResetBits(DrivePort_B, CD);

 

    // SET MR TC

    GLCD_SPI_Transmit(0x26);

 

    // set LCD mapping

    GLCD_SPI_Transmit(0x3d);

 

    // set bias ratio

    GLCD_SPI_Transmit(0xec);

 

    // set gain & potentiometer I bajt

    GLCD_SPI_Transmit(0x81);

 

    // set gain & potentiometer II bajt

    GLCD_SPI_Transmit(0x72);    

 

  // start line number

  GLCD_SPI_Transmit(0x40);         

 

    // display enable

  GLCD_SPI_Transmit(0xaf);         

 

    // all pixels ON - aby zobaczyc reakcje

  GLCD_SPI_Transmit(0xa5);

  /*

  GLCD_SPI_Transmit(0XE2);

     //GLCD_delay(30);

  GLCD_SPI_Transmit(0XEb);

     //GLCD_delay(30);

  GLCD_SPI_Transmit(0X24);

     //GLCD_delay(30);

  GLCD_SPI_Transmit(0X2E);

     //GLCD_delay(30);

  GLCD_SPI_Transmit(0XC4);

     //GLCD_delay(30);

  GLCD_SPI_Transmit(0X89);

     //GLCD_delay(30);

  GLCD_SPI_Transmit(0X81);

     //GLCD_delay(30);

  GLCD_SPI_Transmit(0X20);

     //GLCD_delay(30);

  GLCD_SPI_Transmit(0X40);

     //GLCD_delay(30);

  GLCD_SPI_Transmit(0X30);

     //GLCD_delay(30);

  GLCD_SPI_Transmit(0X22);

     //GLCD_delay(30);

  GLCD_SPI_Transmit(0XAF);

     //GLCD_delay(30);

    GLCD_SPI_Transmit(0xa5);

   //GLCD_delay(30);    

      */         

}

//----------------------------------------------------------------------------------------------------------

void GLCD_SPI_Transmit(char cData) {  

 

    GPIO_SetBits(DrivePort_B, CS);  //CS=1 (ENABLE)

 

    /* Loop while DR register in not empty */

    while( SPI_I2S_GetFlagStatus( GLCD_SPI, SPI_I2S_FLAG_TXE ) == RESET );

    /* Send byte through the SPIx peripheral */

    SPI_I2S_SendData( GLCD_SPI, cData );

  /* Zgodnie z karta katalogowa najpierw trzeba sprawdzic czy bufor nadawczy */

  /* jest pusty a dopiero potem sprawdzac czy SPI skonczylo nadawanie */

  /* Loop while DR register in not empty */

    while( SPI_I2S_GetFlagStatus( GLCD_SPI, SPI_I2S_FLAG_TXE ) == RESET );

  /* Loop while SPI is not busy */

    while( SPI_I2S_GetFlagStatus( GLCD_SPI, SPI_I2S_FLAG_BSY ) == SET );

 

  GPIO_ResetBits(DrivePort_B, CS);        //CS=0 (DISABLE)

 

}

//----------------------------------------------------------------------------------------------------------

void GLCD_HwConfiguration(void)

{

    GPIO_InitTypeDef  GPIO_InitStructure; //Konfiguracja GPIO

  SPI_InitTypeDef   SPI_InitStructure;//Konfiguracja interfejsu SPI

 

  //Enable clocks

  //RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);           //GPIO A Clock

  //RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);            //SPI Clock

 

  //GPIO config

  GPIO_InitStructure.GPIO_Pin = CLK | DIN ;    //SPI: SCK, MISO

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

  GPIO_Init(DrivePort_A, &GPIO_InitStructure);

 

  GPIO_InitStructure.GPIO_Pin = CS | CD | RES; //SPI: CS, CD, RES

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;

    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

  GPIO_Init(DrivePort_B, &GPIO_InitStructure);

 

  //SPI1 Configuration

  SPI_InitStructure.SPI_Direction = SPI_Direction_1Line_Tx;//transmisja jednokierunkowa do MCU

  SPI_InitStructure.SPI_Mode = SPI_Mode_Master;//Tryb pracy SPI, mikrokontroler jako slave

  SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;//8-bit ramka danych

  SPI_InitStructure.SPI_CPOL = SPI_CPOL_High;//Stan Sygnalu taktujacego przy braku transmisji

  SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge;//Aktywne zbocze sygnalu taktujacego

  SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;//Sprzetowa obsluga lini NSS(CS)

  SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_256;//Prescaler, Szybkosc transmisji

  SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;//Pierwszy bit w danych najbardziej znaczacy albo LSB

//  SPI_InitStructure.SPI_CRCPolynomial = 7;//Konfiguracja wielomianu do obliczenia CRC

    SPI_Init(GLCD_SPI, &SPI_InitStructure);//Inicjalizacja SPI

 

  SPI_Cmd(GLCD_SPI, ENABLE);                                         //SPI1 Enable                                             

}

//----------------------------------------------------------------------------------------------------------

void GLCD_delay(unsigned int t)

{

unsigned int i,j;

for(i=0;i<t;i++)

  for(j=0;j<104;j++);

}

//---------------------------------------------------------------------------------------------------------- logic analyzer:

#spi-uc1608
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
ramsamyangelique
Associate
Posted on October 26, 2014 at 15:50

Hi there

 

do you by any chance have your complete code for the lcd uc1608 spi s8 (i am interested in viewing the way you write to the lcd)

thank you