2015-11-20 8:37 AM
Hi All,
I have recently moved over to using a Segger J-Link JTAG adapter. I'm using JLinkGDBServer, ARM Tools GDB in eclipse. The device on my target hardware is an STM32F427II. It appears that I only have R/W access to the SRAM and have Read access to CCMRAM and BKSPRAM. I'm trying to enable Write access to these memory areas.I have a break point setup and a structure already initialised by the processor in BKSPAM. I see the structure in the expressions view.I'm sending gdb the following command: set mem inaccessible-by-default offto force access to the entire memory space. From the gdb console I've also tried: mon info memTo see what memory ranges the server has enabled for the device. It returns: Target does not support this command.I've looked for further device configuration files in the installation folder but none seem to be associated with JLinkGDBServer.I appreciate any assistance in enabling write access to these memory ranges,Best Reagards, Kirem