cancel
Showing results for 
Search instead for 
Did you mean: 

It seems that the Cortex-M3/M4 controllers with EEPROM are being phased out. Is there a reason for this and what are the recommended alternatives?

SSimm.6
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
waclawek.jan
Super User

AFAIK only the 'L0 and 'L1 famiilies have what ST calls EEPROM, i.e. no Cortex-M4-based STM32.

The STM32L1xx family, while NRND, is still under the 10-year commitment, so they should be around for some time.

The alternatives are

  • use RAM with battery-backup
  • use external EEPROM or any similar technology (e.g. FRAM)
  • use the FLASH in a fashion emulating EEPROM

Optimal choice is given by particular requirements of given application.

JW

Probably because the structures are large and hard to manufacture, and don't scale well into new processes?​

T​he goal is to make small low cost general purpose MCU, with high wafer yields, easy to test, and not to combine specialized and incongruant technologies.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

The preferred method would be to use a RAM technology that is sustained with a battery or supercap at very low currents​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
WojtekP1
Associate III

Use flash and just invent something to spread wear right for your use case.