cancel
Showing results for 
Search instead for 
Did you mean: 

Issues with Teseo Suite and Teseo VIC3DA EVB

ADrag.2
Associate II

I'm trying to figure out how to configure the device using the NMEA packet scripts available in Teseo Suite. The problem I'm facing is every one of my PSTMSETPAR packets is being met with an error, even when using the example scripts provided.

I am receiving the NMEA packets properly, but the device won't allow me to make any configurations.

Here's a screenshot of the responses:

https://i.gyazo.com/2ad5429b28fab228ea9a36e7b38cdd1b.png

The script I'm using is labeled "STA9100_5_8_9_GNSS@10Hz-RTCM3_scenario_0". I've also tried a bunch of the other example scripts and all of them give me errors. I've also tried NMEA protocol 3.x and 4.10.

Here's my device configuration: https://i.gyazo.com/f44e592009838c5c36d36fe88b3101de.png

Any advice would be much appreciated.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0