cancel
Showing results for 
Search instead for 
Did you mean: 

Is this an ARM cortex-M4 based board?

rezaelectronicss
Associate II
Posted on September 10, 2016 at 06:56

Hello

I have bought this board about 3-4 year ago and didn't work with, and now I found it in my store and think this has stm32-f407-vgtb microcontroller on it, that I thought it's cortex-M3, but when I searched I found that this is M4 based boared! Is this true?

I have lost anythings of the boards and like to know which things I need to work with this work and where can I find them?

Also, my board number is MB997B, but most of them have MB997A or MB997C when I searched on the internet! what is the difference?

thanks!

http://uupload.ir/files/w261_20160910_083833.jpg

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on September 10, 2016 at 16:53

Yes it is a Cortex-M4 based processor.

The board is an STM32F4-DISCOVERY Rev B, its design and function is going to be very similar to that of Rev A-D. You might want to review specific notations in the User Manual / Schematic for the board.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..