cancel
Showing results for 
Search instead for 
Did you mean: 

Is there a problem with the FIFO of the SDIO?

stm322
Associate II
Posted on March 05, 2009 at 23:01

Is there a problem with the FIFO of the SDIO?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
stm322
Associate II
Posted on May 17, 2011 at 13:05

Hello,

Could somebody confirm or explain where I am wrong with the following problem on a STM32F103ZET6 ?

1 – Can we only write once to the FIFO of the SDIO when DPSM is enabled? And Does the DPSM have to be enabled to write to the FIFO?

2 – Does this problem explain why we can only transfer data with 1 byte block (see errata section 2.13 Limited multibyte support with SDIO cards)

/* SDIO configuration */

SDIO_InitStructure.SDIO_ClockDiv = (UI8)0x01;

SDIO_InitStructure.SDIO_ClockEdge = SDIO_ClockEdge_Rising;

SDIO_InitStructure.SDIO_ClockBypass = SDIO_ClockBypass_Disable;

SDIO_InitStructure.SDIO_ClockPowerSave = SDIO_ClockPowerSave_Disable;

SDIO_InitStructure.SDIO_BusWide = SDIO_BusWide_4b;

SDIO_InitStructure.SDIO_HardwareFlowControl = SDIO_HardwareFlowControl_Disable;

SDIO_Init(&SDIO_InitStructure);

/* “FIFO� configuration with DPSM disabled */

SDIO_DataInitStructure.SDIO_DataTimeOut = SD_DATATIMEOUT;

SDIO_DataInitStructure.SDIO_DataLength = 32;

SDIO_DataInitStructure.SDIO_DataBlockSize = SDIO_DataBlockSize_32b;

SDIO_DataInitStructure.SDIO_TransferDir = SDIO_TransferDir_ToCard;

SDIO_DataInitStructure.SDIO_TransferMode = SDIO_TransferMode_Block;

SDIO_DataInitStructure.SDIO_DPSM = SDIO_DPSM_Disable;

SDIO_DataConfig(&SDIO_DataInitStructure);

/* try to write data in the FIFO */

SDIO_WriteData(0x00000001);

SDIO_WriteData(0x00000002);

SDIO_WriteData(0x00000003);

SDIO_WriteData(0x00000004);

/* RESULT */

/* reading the memory from 0x40018080 to 0x400180FC (FIFO address) everything is at 0, nothing is written */

/* other “FIFO� configuration with DPSM enabled */

SDIO_DataInitStructure.SDIO_DPSM = SDIO_DPSM_Enable;

SDIO_DataConfig(&SDIO_DataInitStructure);

/* try to write data in the FIFO */

SDIO_WriteData(0x00000005);

/* RESULT */

/* reading the memory from 0x40018080 to 0x400180FC (FIFO address). The full FIFO is written with 0x00000005 */

/* try to write again in the FIFO */

SDIO_WriteData(0x00000006);

/* RESULT */

/* reading the memory from 0x40018080 to 0x400180FC (FIFO address). The full FIFO is STILL written with 0x00000005 */

/* reinit DPSM */

SDIO_DataInitStructure.SDIO_DPSM = SDIO_DPSM_Enable;

SDIO_DataConfig(&SDIO_DataInitStructure);

/* try to write data in the FIFO */

SDIO_WriteData(0x00000007);

/* RESULT */

/* reading the memory from 0x40018080 to 0x400180FC (FIFO address). The full FIFO is written with 0x00000007 */

/* try now to access the FIFO with pointer at different address */

UI32 *ptFifo;

ptFifo = (UI32)0x40018084;

/* reinit DPSM */

SDIO_DataInitStructure.SDIO_DPSM = SDIO_DPSM_Enable;

SDIO_DataConfig(&SDIO_DataInitStructure);

/* try to write data in the FIFO */

*ptFifo = 0x00000008;

/* RESULT */

/* reading the memory from 0x40018080 to 0x400180FC (FIFO address). The full FIFO is written with 0x00000008 */

INFO: seeing the behaviour of the FIFO, I didn’t check any registers such as SDIO FIFO Counter. Because DPSM is enabled, as soon as I write to the FIFO, data are transferred.

Thanks in advance.

talib
Associate
Posted on May 17, 2011 at 13:05

I am also facing the same problem with FIFO in SDIO.

is it a known issue in STM32F103 series. What is the work around?