2026-03-30 2:32 AM
As asked in the subject: Is there a hole in the memory map of the STM32C552VC (Bank1 from 0x08000000 to 0x08020000 / Bank2 from 0x08040000 to 0x08060000) or are the two banks continuous from 0x08000000 to 0x08040000)
Solved! Go to Solution.
2026-03-30 2:43 AM - edited 2026-03-30 2:45 AM
Hello,
They are not contiguous in 256K devices:
Bank1 finishes at 0x0801FFFF, Bank 2 starts at 0x08040000
2026-03-30 2:43 AM - edited 2026-03-30 2:45 AM
Hello,
They are not contiguous in 256K devices:
Bank1 finishes at 0x0801FFFF, Bank 2 starts at 0x08040000