2020-12-16 1:07 AM
_vLoadAdd = LOADADDR(.vdata);
.vdata :
{
. = ALIGN(4);
_startvdata = .; /* create a global symbol at data start */
/********** Enable this part when FACTORY is defined *************/
// *\file*.o(.data .data*)
/**************************************************************************************/
. = ALIGN(4);
_endvdata = .; /* define a global symbol at data end */
} >RAM AT> FLASH
In above linker script section my file.o should be include when my FACTORY macro is enabled in make file.
@Community member , Can you please suggest me an example or any workaround?
2020-12-16 2:01 AM
I’m conditionally preprocess linker scripts using the C preprocessor (e.g. arm-none-eabi-cpp). It’s provided by the GCC tool chain as stand-alone executable.
Conditional parts can be handled by preprocessor directives like #ifdef etc.
#include of other/common linker script parts is also possible this way.
That can be easily integrated into a makefile.