cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7/LWIP: IP Ping Error

Hi Community, 

I'm a new Developer/ for ST Microcontrollers, Now Im currently using STM32H723ZGT6 (NUCLEO - 144). Im currently working on ethernet (LWIP), the ping is not working for this code that i have generated . I have seen some youtube channels but I cant rectify and make the ping, I have tried all the possible things like , flash linker script , enabling ICache , Dcache , using MPU(Memory Protection Unit), change them to static ip for both board and my PC and So on . I have tried but I dont know whether my code or my implementation is correct or not . Can anybody help me with this ?..

I have attached the file thats my code and how project. pls have a look into that. 

Thank You. 

5 REPLIES 5
mƎALLEm
ST Employee

Hello @Gokul_Sarvanakumar_60 and welcome to the ST community,

How to create a project for STM32H7 with Ethernet and LwIP stack working

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Thank You for the reply still its not working, I cant identify the issue. 

I'm almost sure you didn't follow the exact steps described in the knowledge base article.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Pavel A.
Super User

yes these pre- configured are perfectly working.  but my own code is not working