cancel
Showing results for 
Search instead for 
Did you mean: 

Interrupt routine not called STM324x9I-Eval

Beck.Karl-Michael
Associate III
Posted on March 25, 2015 at 18:18

Hi,

i'm pretty new to Interrupt handling so maybe i forgot something. This is my code for Setting up PA0 & PA1 Input Pins. The pin state works fine:

bool GetRegisterDdkSpurA() { return GPIOA->IDR & GPIO_IDR_IDR_0; }   

bool GetRegisterDdkSpurB() { return GPIOA->IDR & GPIO_IDR_IDR_1; } 

but i get no call of the Interrupt Routine - i set up like this:

__GPIOA_CLK_ENABLE();

// GPIO A, Pin 0 Init               

static GPIO_InitTypeDef aGpioInitPin0;               

aGpioInitPin0.Mode = GPIO_MODE_INPUT;           

aGpioInitPin0.Pull = GPIO_PULLDOWN;

aGpioInitPin0.Speed = GPIO_SPEED_LOW;

aGpioInitPin0.Alternate = 0;           

aGpioInitPin0.Pin = GPIO_PIN_0;               

HAL_GPIO_Init(GPIOA, &aGpioInitPin0);

// GPIO A, Pin 1 Init               

static GPIO_InitTypeDef aGpioInitPin1;               

aGpioInitPin1.Mode = GPIO_MODE_INPUT;

aGpioInitPin1.Pull = GPIO_PULLDOWN;

aGpioInitPin1.Speed = GPIO_SPEED_LOW;

aGpioInitPin1.Alternate = 0;           

aGpioInitPin1.Pin = GPIO_PIN_1;               

HAL_GPIO_Init(GPIOA, &aGpioInitPin1);

                                  

// Interrupt for PA0

SYSCFG->EXTICR[0] = (SYSCFG->EXTICR[0] & SYSCFG_EXTICR1_EXTI0) | SYSCFG_EXTICR1_EXTI0_PA;    // Port A, Pin 0 auf _EXTI0-interrupt mappen.                           

EXTI->RTSR |= (1 << EXTI0_IRQn);                                                             // Enable Rising Trigger for Interrupt ExtI0

EXTI->FTSR |= (1 << EXTI0_IRQn);                                                             // Enable Fallig Trigger for Interrupt ExtI0

HAL_NVIC_SetPriority(EXTI0_IRQn, 0x0F, 0x00);                                                // lowest priority.           

HAL_NVIC_EnableIRQ(EXTI0_IRQn);                                                              // enable interrupt.         

// Interrupt for PA1

SYSCFG->EXTICR[1] = (SYSCFG->EXTICR[1] & SYSCFG_EXTICR1_EXTI1) | SYSCFG_EXTICR1_EXTI1_PA;    // Port A, Pin 1 auf _EXTI1-interrupt mappen.                           

EXTI->RTSR |= (1 << EXTI1_IRQn);                                                             // Enable Rising Trigger for Interrupt ExtI1

EXTI->FTSR |= (1 << EXTI1_IRQn);                                                             // Enable Fallig Trigger for Interrupt ExtI1

HAL_NVIC_SetPriority(EXTI1_IRQn, 0x0F, 0x00); // lowest priority.           

HAL_NVIC_EnableIRQ(EXTI1_IRQn); // enable interrupt.         

extern ''C'' void EXTI0_IRQHandler(void)

{

  // ...

}

extern ''C'' void EXTI1_IRQHandler(void)

{

  // ...

}

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0