cancel
Showing results for 
Search instead for 
Did you mean: 

Interplay of DFU bootloader and Applikation

frankpoppen9
Associate
Posted on November 24, 2011 at 11:25

Sorry for posting this as newbe, but I'm browsing all the PDFs I found and used all the search queries relevant on this forum without result. My Problem inshort first and then long.

SHORT:

-Purchased evaluation board STM3210B-EVAL

-downloaded um0435.zip (STM3210B-EVAL_FW_V2.0.0)

-downloaded included DFU with DfuSeDemo.exe (OK!)

-used file manager DFU -> HEX and then back HEX -> DFU. after download still (OK!) - Conclusion files and tools are working properly.

Problem:

- Opening the RIDE project of Demo (STM3210B-EVAL_Demo.rprj). Version 7.30.10.0159

- build is OK, HEX generated. HEX -> DFU OK

- after upload device does not leave DFU mode after RESET. (Leaves, but goes right back into it).

Assumption: Generated HEX does not work with bootloader. Startaddress wrong (or so?) How to generate HEX that works with DFU bootloader? Why does the demo not work out of the box as should be (for a Demo!)? Thanks for any help and link to further

documentation.

Longer Comment:

I can sucessfully download the delivered demo application HEX to the evaluation board and have the nice slide show etc running. But if I compile the delivered demo from delivered source and RIDE project (runs without problem) the generated HEX converted to DFU does still dowload, but is not started. The device always goes back to DFU mode.

Reading everything I found I today believe that my application should start at address 0x800003000? But why is the demo projects configured at 0x800000000? Or should it be there? I do not see a way to change the startaddress in the RIDE7 development tool.

Somewhere here must be a nice ''How to start your HelloWorld with DFU bootloader!'' but I'm not able to find it, sorry.

Thanks for any help.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
stforum.tormod9
Associate II
Posted on November 25, 2011 at 10:37

I think you have understood it correctly: The demo applications can be run standalone (and must then start at 0x08000000) or can be used with the DFU bootloader in which case they will have to start at 0x08003000, where the DFU bootloader expects to find them. The boot loader itself resides at 0x08000000 of course. You should verify the application start address in the DFU code, some modified bootloaders might look for the application at for instance 0x08004000 instead.

The demo applications probably build out-of-the-box for standalone operation. So if you want to use them with DFU you have to the change the start address. Usually that is a linker option (or specified in a linker file). You will have to read your RIDE documentation to see how it is done there.

Note also that the application might refer to its start location, for instance in calls to NVIC_SetVectorTable(), so this must be adjusted too.

HTH,

Tormod