2012-05-14 8:40 AM
hi,
i am working on the stm32discovery i am trying to increment a timer (timer2 channel 1) each time the signal on the pin PA.05 is rising but the timer is random incrementing and not at each rising edge of the signal i don't understand why ? here is my code : int main(void) { /* Configure Clocks for Application need */ RCC_Configuration(); /* Configure RTC Clocks */ //RTC_Configuration(); /* Configure SysTick IRQ and SysTick Timer to generate interrupts every 500µs */ RCC_GetClocksFreq(&RCC_Clocks); //SysTick_Config(RCC_Clocks.HCLK_Frequency / 2000); /* Enable GPIOs clock */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2,ENABLE); RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA,ENABLE); /*PA.05 TIM2 channel 1*/ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_40MHz; GPIO_Init(GPIOA,&GPIO_InitStructure); GPIO_PinAFConfig(GPIOA, GPIO_PinSource5, GPIO_AF_TIM2); TIM_InitStruct.TIM_Period = 849; TIM_InitStruct.TIM_Prescaler = 0; TIM_InitStruct.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM2,&TIM_InitStruct); /*timer2 chanel 1 ETR pin PA5*/ TIM_ICInitStruct.TIM_Channel = TIM_Channel_1; TIM_ICInitStruct.TIM_ICPolarity = TIM_ICPolarity_Rising; TIM_ICInitStruct.TIM_ICSelection = TIM_ICSelection_DirectTI; TIM_ICInitStruct.TIM_ICPrescaler = TIM_ICPSC_DIV1; TIM_ICInitStruct.TIM_ICFilter = 0x0; TIM_ICInit(TIM2, &TIM_ICInitStruct); /*enable the TIM counter*/ TIM_Cmd(TIM2, ENABLE); TIM_TIxExternalClockConfig(TIM2, TIM_TIxExternalCLK1Source_TI1, TIM_ICPolarity_Rising, 0); TIM_ETRClockMode1Config(TIM2,TIM_ExtTRGPSC_OFF, TIM_ExtTRGPolarity_NonInverted,0); while (1){ SysTick_Config(RCC_Clocks.HCLK_Frequency / 2000); bitStatut = GPIO_ReadInputDataBit(GPIOA, GPIO_Pin_5); increment = TIM_GetCapture1(TIM2); Delay(100); } could you help me ? thanks2013-02-25 9:21 AM
Bonding PC6 to PA0 button input
void TIM3_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC | RCC_APB2Periph_AFIO, ENABLE); // AFIO required for remapping
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6; // PC6 TIM3_CH1
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;
GPIO_Init(GPIOC, &GPIO_InitStructure);
GPIO_PinRemapConfig(GPIO_FullRemap_TIM3, ENABLE);
TIM_TimeBaseStructure.TIM_Period = 65535;
TIM_TimeBaseStructure.TIM_Prescaler = 0;
TIM_TimeBaseStructure.TIM_ClockDivision = 0;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure);
TIM_TIxExternalClockConfig(TIM3, TIM_TIxExternalCLK1Source_TI1, TIM_ICPolarity_Rising, 0);
TIM_Cmd(TIM3, ENABLE);
}
2013-02-25 11:16 AM
Big THANK YOU! It was the RCC_APB2Periph_AFIO that solved my issue! You saved me alot of time.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.