2012-05-10 8:07 AM
Hi, I am using STM32F105RB and I have a problem with an I2S master receive connection, using SPI2.
I have configured SPI2 in I2S master Receiver mode, and enabled a SPI2 receive interrupt but immediately after SPI2 initialization in I2S mode I am getting Receive interrupt continuously. SPI2 init. function and I2S2 IRQ handler.. VOID I2S_2_Init( VOID ) { GPIO_InitTypeDef GPIO_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; I2S_InitTypeDef I2S_InitStructure; // Clock configurations /* SPI3 and SPI2 clocks enable */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI3 | RCC_APB1Periph_SPI2, ENABLE); // NVIC Config /* SPI2 IRQ channel configuration */ NVIC_InitStructure.NVIC_IRQChannel = SPI2_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); // GPIO config /* Configure SPI2 pins: CK, WS and SD ---------------------------------*/ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12 | GPIO_Pin_13 | GPIO_Pin_15; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOB, &GPIO_InitStructure); // I2S config /* I2S peripheral configuration */ SPI_I2S_DeInit(SPI2); I2S_InitStructure.I2S_Standard = I2S_Standard_PCMShort; I2S_InitStructure.I2S_DataFormat = I2S_DataFormat_16b; I2S_InitStructure.I2S_MCLKOutput = I2S_MCLKOutput_Disable; I2S_InitStructure.I2S_AudioFreq = I2S_AudioFreq_8k; I2S_InitStructure.I2S_CPOL = I2S_CPOL_Low; I2S_InitStructure.I2S_Mode = I2S_Mode_MasterRx; // I2S2 as master RX I2S_Init(SPI2, &I2S_InitStructure); /* Enable the I2S2 RxNE interrupt */ SPI_I2S_ITConfig(SPI2, SPI_I2S_IT_RXNE, ENABLE); // RX Int. /* Enable the I2S2 */ I2S_Cmd(SPI2, ENABLE); STM_EVAL_LEDToggle(LED1); // NC } /* IRQ handlear */ VOID SPI2_IRQHandler ( VOID ) { STM_EVAL_LEDToggle(LED2); // NC /* Check the interrupt source */ /* RX */ if (SPI_I2S_GetITStatus(SPI2, SPI_I2S_IT_RXNE) == SET) { STM_EVAL_LEDToggle(LED3); // NC /* Store the I2S2 received data in the relative data table */ usnI2SDatBuf[ucIndex++] = SPI_I2S_ReceiveData(SPI2); } } #i2s-spi-interrupts-interrupWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.