cancel
Showing results for 
Search instead for 
Did you mean: 

I have an STM32429I-EVAL board purchased.

GKV.1
Associate

I have an STM32429I-EVAL board purchased. The board has CN6 and CN7 MALE extension headers of 1.27mm pitch, the standard jumper wire will fit with 2.54mm pins for evaluation and checking the MCU programs. What should I do to connect a jumper wire to the CN6 and CN7 Male headers. Kindly Suggest a suitable jumper wire with part no. or a suitable pin pitch changer so that signals can be taken for evaluation during MCU programming. Suggest a suitable product for the problem. Thank you

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0