I can't ensure SPI communication between STM32F4 board and Eval-STPM34 metrology board !!!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-03-28 8:12 AM
Hi,
I want to ensure SPI communication between STM32F407VG board and Eval-STPM34 metrology board , i am trying to read just a register of the Eval-STPM34 but i always fail , i used these pins to ensure the SPI communication :
STM32 -----> EVAL-STPM34
MOSI-----> MOSI
MISO-----> MISO
SCL -----> SCL
PC1 -----> SCS
PC2 -----> SYN
PC3 -----> EN
PA0 -----> LED2
GND -----> GND
VCC -----> VCC
And i made the CubeMX configuration below ....
I found in the datasheet and user manual of STPM34 that i have to initialize the STPM34 :
1-"If the SCS is set low and EN pin goes from low to high, the STPM32 communicates by SPI
mode. If the SCS is set high and EN pin goes from low to high, the STPM32 communicates
by UART mode. The STPM32 EN pin can be tied to VDD thanks to a pull-up if it is not
driven (EVALSTPM32 board). In this case, no additional wire between the STM32F103RD
and the STPM32 is needed.
EN pin can be also driven by FW:
- Put EN low to reset the configuration
- Set the desired level on SCS (for SPI or UART)
- Put EN high level to latch the configuration "
i want a SPI communication so i edited this code :
HAL_GPIO_WritePin(GPIOC,GPIO_PIN_3,GPIO_PIN_RESET); //Reset EN
DWT_Delay_us(1000);
HAL_GPIO_WritePin(GPIOC,GPIO_PIN_1,GPIO_PIN_RESET); //Reset SCS
DWT_Delay_us(1000);
HAL_GPIO_WritePin(GPIOC,GPIO_PIN_3,GPIO_PIN_SET); //Set EN
2-i found also that i must initialize SYN
"As mentioned in the STPM34 datasheet, after the POR, the chip must be reset by toggling
3 times SYN pin and once SCS pin."
and you find the sequence of reset below ......
So i edited this code :
HAL_GPIO_WritePin(GPIOC,GPIO_PIN_1,GPIO_PIN_SET); //SET SCS
HAL_GPIO_WritePin(GPIOC,GPIO_PIN_2,GPIO_PIN_SET); //SET SYN
for(uint8_t i=0;i<=2; i++)
{
HAL_GPIO_WritePin(GPIOC,GPIO_PIN_2,GPIO_PIN_RESET); //Reset SYN
DWT_Delay_us(100);
HAL_GPIO_WritePin(GPIOC,GPIO_PIN_2,GPIO_PIN_SET); //Set SYN
DWT_Delay_us(100);
}
HAL_GPIO_WritePin(GPIOC,GPIO_PIN_1,GPIO_PIN_RESET); //Reset SCS
DWT_Delay_us(100);
HAL_GPIO_WritePin(GPIOC,GPIO_PIN_1,GPIO_PIN_SET); // SET SCS
3-And finally i want to read the register row 2 which it default value is 0x000004E0 , it address is 0x04 as mentionned in the datasheet of STPM34 so i edited this code :
spi_txbuff[0]=0x04; //buffer contains adress of the register
HAL_GPIO_WritePin(GPIOC,GPIO_PIN_1,GPIO_PIN_RESET); //RESET SCS
HAL_SPI_Transmit(&hspi1,spi_txbuff,1,50); //Send register adress
HAL_SPI_Receive(&hspi1,spi_rxbuff,4,50); //Read register data (4 bytes)
HAL_GPIO_WritePin(GPIOC,GPIO_PIN_1,GPIO_PIN_SET); //SET SCS
And unfortunately in debugging mode i always find : 0xFF 0xFF 0xFF 0xFF
Wish your help,please!!
- Labels:
-
SPI
-
STM32F4 Series