cancel
Showing results for 
Search instead for 
Did you mean: 

[HW] Direct connect between Ports of STM32s?

gds23
Associate II
Posted on July 13, 2011 at 05:51

If two STM32 devices are wired together in a system, is it necessary to place fairly small series resistors between the port connection to limit the current in case a port or ports somehow starts driving current to the other processor and possibly degrades or destroys it? This is not a big problem to do except that the series resistance somewhat reduces the maximum SPI baudrate between the STM32 parts, e.g., can go 18Mbps w/o resistors but only 9Mbps works with the resistors on the SPI signals.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Andrew Neil
Super User
Posted on July 13, 2011 at 07:59

''If two STM32 devices are wired together in a system, is it necessary to place fairly small series resistors between the port connection''

 

No, it's not necessary.

''in case a port or ports somehow starts driving current to the other processor''

 

 

Just be careful to ensure that doesn't happen!

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.