cancel
Showing results for 
Search instead for 
Did you mean: 

How to reload STM3210C-EVAL demo firmware?

mschwab
Associate II
Posted on June 03, 2011 at 19:43

I just got my STM3210C-EVAL board.  I loaded the I/O Expander and other demo apps, but now I can't get back to the original Demo firmware (with the GUI with 5 icons).  When I load the project in Keil is has no source code, can't compile, and when I go into Debug it appears to be loading a HEX file, but nothing happens.  The board continues to run whatever example was previously loaded.

Could it be because I'm still using the demo Keil tools (with a 32kb limit)?  It's not complaining like it usually does.

We should be getting the full-licensed version of Keil any day now.

Michael

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0