cancel
Showing results for 
Search instead for 
Did you mean: 

How to perform CQ overload test using l6360.

SNAGU.1
Associate

Hi,

I am using STM32f423RH and l6360.

how to perform CQ overload test..?

I am able to read and write the registers of l6360.

As per my understanding from the data sheet, CQ overload will happen when the CQ line reaches the cutoff (programmed cutoff) then the CQ overload bit will be set.

i have programmed cutoff current as 220 mA.

To simulate this test i am using a load bank and setting 225mA and i am reading the status register. the status register is empty and giving the value 0.

Please can anyone help me to do this test.

any help will be appreciated.

Thanks in advance.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0