2018-02-05 6:38 PM
Hello.
I am in trouble with connecting virtual comport in STM32 to PC.
I think that the virtual comport is properly working in the MCU, and it is well communicated with TeraTerm (the serial port communication application in PC).
Now, I am coding for serial port in C++ and C# for the comport, but an error or exception occurred with serial port error code 87.
C code.
BuadRate = CBR_115200
ByteSize = 8
fParity = FALSE;
Parity = NOPARITY
StopBits = ONESTOPBIT
bool CSerialPort::configurePort(DWORD BaudRate, BYTE ByteSize, DWORD fParity,
BYTE Parity, BYTE StopBits){ if ((m_bPortReady = GetCommState(m_hComm, &m_dcb)) == 0) { MessageBox(NULL, 'GetCommState Error', 'Error', MB_OK + MB_ICONERROR); CloseHandle(m_hComm); return false; }m_dcb.BaudRate = BaudRate;
m_dcb.ByteSize = ByteSize; m_dcb.Parity = Parity; m_dcb.StopBits = StopBits; m_dcb.fBinary = true; m_dcb.fDsrSensitivity = false; m_dcb.fParity = fParity; m_dcb.fOutX = false; m_dcb.fInX = false; m_dcb.fNull = false; m_dcb.fAbortOnError = true; m_dcb.fOutxCtsFlow = false; m_dcb.fOutxDsrFlow = false; m_dcb.fDtrControl = DTR_CONTROL_DISABLE; m_dcb.fDsrSensitivity = false; m_dcb.fRtsControl = RTS_CONTROL_DISABLE; m_dcb.fOutxCtsFlow = false; m_dcb.fOutxCtsFlow = false;m_bPortReady = SetCommState(m_hComm, &m_dcb); // <= Error occurs
if (m_bPortReady == 0)
{ CString str1; str1.Format(_T('%d'), GetLastError()); MessageBox(NULL, str1, 'error', MB_OK); CloseHandle(m_hComm); return false; } return true;}2. C# Code
SerialPort port = new SerialPort('COM2', 115200, Parity.None, 8, StopBits.One);
port.ReadTimeout = 1000; port.WriteTimeout = 1000; try { port.Open(); } catch (Exception exp) { Console.WriteLine(exp.ToString()); }We’re moving the ST Community to a new platform to give you a better and more reliable community experience.