2018-12-06 10:45 AM
So, There are two sourse of clocks in STM32.
1) Inner RC generator
2) External crystal.
I need to use second variant. I use asm.
I determined the address responsible for choosing the source of clocking. The address is 0x40023800. I wrote down the value of 0x00050000 at this address.
But the clock source does not change. The microcontroller uses an internal clock source.
What is a solution to this problem?
2018-12-06 11:30 AM
I don't know what part you are using.
I don't know how your code is working.
Try again
>>What is a solution to this problem?
Review the RM more carefully. Review what the C code and other libraries are doing in the context of what you're learnt from the RM
>> I wrote down the value of 0x00050000 at this address.
So perhaps enabled the HSE in BYPASS mode, where's it routed after that?
2018-12-07 12:26 AM
Thanks!
My code:
#define RCC_control_register *(unsigned long*)(0x40023800)
#define HSI_ON 0
#define HSE_ON 16
#define HSE_READY_FLAG 17
#define HSE_BYPASS 18
void pause (int time){
for (int i=0; i!=time; i++){
}
}
int main(){
// Step #1: HSE turn on
RCC_control_register |= (1 << HSE_ON)|(1 << HSE_BYPASS);
//Step @2: HSI turn off
RCC_control_register &=! (1 << HSI_ON);
//Step #3: delay for 5 clock of MCU
asm("NOP");
asm("NOP");
asm("NOP");
asm("NOP");
asm("NOP");
// Step #4: Ready the flag of stable clock
while (!(RCC_control_register & (HSE_READY_FLAG)) == (1 << HSE_READY_FLAG));
const int timeOfPause = 1000000;
*(unsigned long*)(0x40023830) |= 0x8;
asm("NOP");
asm("NOP");
asm("NOP");
*(unsigned long*)(0x40020C00) = 0x55550000;
*(unsigned long*)(0x40020C04) = 0;
*(unsigned long*)(0x40020C08) = 0;
*(unsigned long*)(0x40020C0C) = 0;
while (1){
*(unsigned long*)(0x40020C14) = 0xF000;
pause (timeOfPause);
*(unsigned long*)(0x40020C14) = 0x0000;
pause (timeOfPause);
*(unsigned long*)(0x40020C14) = 0x1000;
pause (timeOfPause);
*(unsigned long*)(0x40020C14) = 0x2000;
pause (timeOfPause);
*(unsigned long*)(0x40020C14) = 0x4000;
pause (timeOfPause);
*(unsigned long*)(0x40020C14) = 0x8000;
pause (timeOfPause);
for (int k=0; k!=10; k++){
*(unsigned long*)(0x40020C14) = 0x1000;
pause(timeOfPause);
*(unsigned long*)(0x40020C14) = (*(unsigned long*)(0x40020C14) << 1);
pause(timeOfPause);
*(unsigned long*)(0x40020C14) = (*(unsigned long*)(0x40020C14) << 1);
pause(timeOfPause);
*(unsigned long*)(0x40020C14) = (*(unsigned long*)(0x40020C14) << 1);
pause(timeOfPause);
}
}
}MCU use inner RC generator, not external