cancel
Showing results for 
Search instead for 
Did you mean: 

How many Max Slaves in SPI

Muzahir Hussain
Associate III
Posted on February 02, 2018 at 10:19

In SPI protocol, how many  maximum slaves can I connect to master(nucleo STM32F103RB)?

#stm32f103rb #spi-communication #nucleo-stm
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
AvaTar
Lead
Posted on February 02, 2018 at 11:52

Basically, SPI was intended as point-to-point protocol, i.e. one master, one slave.

You can add more slaves by using more or less elaborate Slave-Select mechanisms, that selects one slave out of <n>.

However, when using software slave select, you might run into trouble using interrupts or DMA for transfers.