cancel
Showing results for 
Search instead for 
Did you mean: 

How is pmaadress calculated in HAL_PCDEx_PMAConfig?

dani
Associate
Posted on November 25, 2016 at 10:03

Generating USB CDC example in STM32CubeMX for STM32F103 it creates the following code inside

USBD_LL_Init

():

HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x00 , PCD_SNG_BUF, 0x18);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x80 , PCD_SNG_BUF, 0x58);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x81 , PCD_SNG_BUF, 0xC0);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x01 , PCD_SNG_BUF, 0x110);
HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x82 , PCD_SNG_BUF, 0x100);

How are 0x18, x058, x0C0... calculated? I get that they are endpoint positions inside PMA buffer, but could not find the exact calculation. I read RM0008, ''3 USB functional description'' , the closest I get is ''Figure Packet buffer areas with examples of buffer description table locations''
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
slimen
Senior
Posted on November 29, 2016 at 15:04

Hello,

Refer to this

http://www.st.com/content/ccc/resource/technical/document/user_manual/01/c6/32/df/79/ad/48/32/CD00158241.pdf/files/CD00158241.pdf/jcr:content/translations/en.CD00158241.pdf

: STM32 USB-FS-Device development kit, maybe this helps you.

Regards

Geoffrey1
Senior
Posted on December 12, 2016 at 03:05

I'm surprised nobody seems to have an answer.  This is definitely not documented either in the Cube HAL or (at least for the stm32f3) reference manual.   Without this key bit of information, it is virtually impossible to build a USB device that doesn't simply used the (rather limited) standard examples.