cancel
Showing results for 
Search instead for 
Did you mean: 

How I can implement MQTT protocol stack on STM32 with GSM module simcom7100E ?

sunil sahu
Associate
Posted on March 16, 2018 at 12:11

Hi

I want to use SIMCOM7100E GSM module with STM32 board with MQTT protocol stack embedded on it.

Is there any STM32 development board or any STM Development board which supports MQTT protocol stack with simcom7100E GSM module?

?

#simcom7100e+mqtt+stm32+gsm
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Andrew Neil
Super User
Posted on March 16, 2018 at 13:35

Always good to search for existing material:

https://community.st.com/search.jspa?q=mqtt

eg,

Like other internet protocols, MQTT is entirely independent of the underlying hardware.

So just try googling something like, 'MQTT microcontroller client'

https://community.st.com/0D50X00009XkX21SAF

Note that ST have recently announced some Cellular Discovery Kits:

https://community.st.com/0D50X00009XkbSJSAZ

Although they may not actually be available yet, check the product pages to see if there's any useful info or software...

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
vuahoa07
Associate II
Posted on May 13, 2018 at 03:57

I  had a similar problem last year and find no implementation. So I write my old TCP handler and mqtt client based on lwip's mqtt.The most important thing is the TCP interface with SIM7100 (through AT). The MQTT is not so difficult to implement.

(Because of company security, i cannot share the source).