cancel
Showing results for 
Search instead for 
Did you mean: 

How do I change the audio file?

dannyschweizer
Associate
Posted on October 05, 2009 at 16:32

How do I change the audio file?

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
dannyschweizer
Associate
Posted on May 17, 2011 at 13:24

Hi,

I've got a question concerning the application note AN2739 (playing audio files with I2S audio codec), using the STM3210E-EVAL board:

When I load the application onto the board, the standard STM32-family-presentation appears. Where is this audio file located and how do I change the audio file playing?

Sorry, if it's a stupid question, I'm not very experienced.

Thank you in advance for your reply!

Danny

tomas23
Associate II
Posted on May 17, 2011 at 13:24

DFU PC installation has DFU file manager in its program folder, that can extract and again create the .dfu files. I guess the wav file is added as binary content, so no trouble at all!

tomas23
Associate II
Posted on May 17, 2011 at 13:24

See page 21 of the AN :D

It's external NOR in the FSMC iface, preloaded with the presentation data.

roger239955
Associate II
Posted on May 17, 2011 at 13:24

Ok the file (wave)is loaded with the DFU demonstration firmware (STM3210E-EVAL_Demo_NORFlash_V2.0.0.dfu) as bin file.

But how do I change the audio file ?

It is a binary file.

How can i change a wave file to a binary file ?

Or how can I store another wave file as the DFU standard wave file ?

greeting

Roger

[ This message was edited by: roger.schweizer on 28-09-2009 10:32 ]