cancel
Showing results for 
Search instead for 
Did you mean: 

Hii..When I try and write the .bin file to the Nucleo's USB drive the USB drive momentarily disconnects from windows and then reconnects but no file has been written to the Nucleo. It is as if the Nucleo's board is write protected.

Gk.1
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

I don't use this method, but it is a faux drive, in that it pretends to be a MSC with FAT File System long enough to accept the file as it writes thru into the STM32's flash space.

I'm not sure it is supposed to allow you to see the .BIN file, but rather something showing a Pass / Fail status.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..